Android browser menu break

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android browser menu break

3,304 Views
weikeng-jimmy
Contributor III

Hi All,google_search.png

I would refresh Browser some times on the Android platform. The Google search web site sometimes menu break occur.
Test environment : Sabre-SD board
BSP version : android_jb4.2.2_1.1.0

How to improve this situation ? Thanks!

Labels (3)
0 Kudos
Reply
6 Replies

3,124 Views
saurabh206
Senior Contributor III

Hi,

To fixed for this issue is needs to update the GPU library.

Please see attached

Android jb4.2.2 GPU upgade with the latest 4.6.9p13 (used in jb4.3)

Thanks

Saurabh

0 Kudos
Reply

3,124 Views
YixingKong
Senior Contributor IV

Jimmy

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

3,124 Views
YixingKong
Senior Contributor IV

Jimmy

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.

Thanks,
Yixing

0 Kudos
Reply

3,124 Views
fabiof
Contributor IV

I have the exact same problem. Same BSP version android_jb4.2.2_1.1.0. Connected to HDMI I can see the problem using hight or low resolutions. In my case is possible to reproduce by fast scrolling up or down a page with some images and a lot of text.


Someone found a workaround?

0 Kudos
Reply

3,124 Views
SergioSolis
NXP Employee
NXP Employee

Is your output to HDMI or LVDS?, what is the resolution of the screen?, i haven't been able to replicate this issue...

0 Kudos
Reply

3,124 Views
weikeng-jimmy
Contributor III

LVDS resolution : 1024x768

You can replicate when touch refresh button quickly .

0 Kudos
Reply