Android and Bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android and Bluetooth

ソリューションへジャンプ
3,276件の閲覧回数
babur
Contributor II

Hi all.

Currently in my project i'm using another mcu to run Android and Drive I2C, UART, GPIO and USB functionalities. Also I should add Bluetooth functionalities to our system. But our BSP Android copy and patch doesn't support bluetooth. It's impossible to enable BT.

So i decided to change all our hardware to freescale's one.

I think i.MX512 is good enough for me. Also i will buy iWave imx51 kit. (It has NAND support)

But i'm not sure if FREESCALE's i.Mx Android sources contain Bluetooth libraries and driver etc.

Also which or what type BT module i must use for i.Mx Development Board and also in future my custom board.

Please give me some information.

Am i correct way?

Many Thanks

Babür SENTURK

Software Eng.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,602件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

Hi Babur

In our latest GB release (R10.3.2), we support athoers AR3K bluetooth(actually a atheros combo for BT/WIFI) for i.MX53.

I think you can easily porting that to i.MX51.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,603件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

Hi Babur

In our latest GB release (R10.3.2), we support athoers AR3K bluetooth(actually a atheros combo for BT/WIFI) for i.MX53.

I think you can easily porting that to i.MX51.

0 件の賞賛
返信
2,602件の閲覧回数
babur
Contributor II

Recently i'm contacting our local FSC provider. They offer iMX502 for us. Also iMX Bluetooth Dongle. I will buy IMX50EVK and the BT dongle.

Thanks

0 件の賞賛
返信