Android UI not fix with lcd display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android UI not fix with lcd display

1,498件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi all,

I'm working on imx6 android 4.4.3 solo board. LCD resolution is 800x480, Android UI not fulfilled with display. Full UI is coming as little small. Some empty space are there only in left and right of the screen. How to make it full??

Regards

Aravinth

0 件の賞賛
返信
1 返信

1,361件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Aravinth,

      The issue should be generated by LCD timing, so you will have to adjust LCD timing according to LCD's datasheet. If you are using LVDS lcd, timing structure is ldb.c( LVDS driver), if your LCD is parallel interface and connected to DISP0 port, timing structure is mxc_lcd.c

regards,

weidong

0 件の賞賛
返信