Android SPI configuration for i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android SPI configuration for i.mx6

2,104 Views
tftu
Contributor III

Hi All,

    I'm testing a device which connecting to MCIMX6Q-SDB board thr. SPI interface based on image_imx-android-13.4.1_6qsabresd as the BSP. Have read some SPI discussion in community, all of them are target for Linux, I still try to follow this discussion thread: https://community.freescale.com/message/309184#309184 and apply below changes in my environment:

1. - #if defined(CONFIG_MTD_M25P80)

    - .modalias = "m25p80",

    + .modalias = "spidev",

    - #endif

2. Enable the SPI user mode driver in by "make manuconfig" and save.

    However, when I return to ~/myandroid folder and trying to make whole project, I got:

============================================

PLATFORM_VERSION_CODENAME=REL

PLATFORM_VERSION=4.0.4

TARGET_PRODUCT=sabresd_6dq

TARGET_BUILD_VARIANT=user

TARGET_BUILD_TYPE=release

TARGET_BUILD_APPS=

TARGET_ARCH=arm

TARGET_ARCH_VARIANT=armv7-a-neon

HOST_ARCH=x86

HOST_OS=linux

HOST_BUILD_TYPE=release

BUILD_ID=UNKNOWN

BUILD_NUMBER=eng.tftu.20131108.190951

============================================

No private recovery resources for TARGET_DEVICE sabresd_6dq

make -C kernel_imx -j4 uImage ARCH=arm CROSS_COMPILE=`pwd`/prebuilt/linux-x86/toolchain/arm-eabi-4.4.3/bin/arm-eabi-

make[1]: Entering directory `/home/tftu/myandroid4.0.4_ForQuad_20131106/kernel_imx'

scripts/kconfig/conf --silentoldconfig Kconfig

*

* Restart config...

*

*

* Linux/arm 3.0.35 Kernel Configuration

*

Patch physical to virtual translations at runtime (EXPERIMENTAL) (ARM_PATCH_PHYS_VIRT) [N/y/?] (NEW)

..... cut ......

             And then it asks me to select all questions as the same in the menuconfig, trying to select default most questions except System Type:

*

* System Type

*

MMU-based Paged Memory Management Support (MMU) [Y/n/?] y

ARM system type

  1. ARM Ltd. Integrator family (ARCH_INTEGRATOR) (NEW)

  2. ARM Ltd. RealView family (ARCH_REALVIEW) (NEW)

> 3. ARM Ltd. Versatile family (ARCH_VERSATILE) (NEW)

  4. ARM Ltd. Versatile Express family (ARCH_VEXPRESS) (NEW)

  5. Atmel AT91 (ARCH_AT91) (NEW)

  6. Broadcom BCMRING (ARCH_BCMRING) (NEW)

  7. Cirrus Logic CLPS711x/EP721x-based (ARCH_CLPS711X) (NEW)

  8. Cavium Networks CNS3XXX family (ARCH_CNS3XXX) (NEW)

  9. Cortina Systems Gemini (ARCH_GEMINI) (NEW)

  10. EBSA-110 (ARCH_EBSA110) (NEW)

  11. EP93xx-based (ARCH_EP93XX) (NEW)

  12. FootBridge (ARCH_FOOTBRIDGE) (NEW)

  13. Freescale MXC/iMX-based (ARCH_MXC) (NEW)

  14. Freescale MXS-based (ARCH_MXS) (NEW)

  15. Hilscher NetX based (ARCH_NETX) (NEW)

..... cut ......

        I select 13. Freescale MXC/iMX-based (ARCH_MXC) (NEW) to fit my board, but the next question, Freescale MXC Implementations, it automatically select MX31 platforms without choices:

*

* Freescale MXC Implementations

*

Freescale CPU family:

  1. MX1-based (ARCH_MX1) (NEW)

  2. MX2-based (ARCH_MX2) (NEW)

  3. MX25-based (ARCH_MX25) (NEW)

> 4. MX3-based (ARCH_MX3) (NEW)

  5. i.MX50 + i.MX53 (ARCH_MX503) (NEW)

  6. i.MX51 (ARCH_MX51) (NEW)

  7. MX6-based (ARCH_MX6) (NEW)

choice[1-7]: 4

*

* MX31 platforms:

*

Support MX31ADS platforms (MACH_MX31ADS) [Y/n/?] (NEW)

         Finally I select default options for the other questions and keep the building, but failed with errors.I have apply the same based on android_jb4.2.2_1.1.0-ga_source but still got the same result.

         My major question is how to config SPI interface in Android, but now it looks like I should figure out above menuconfig issue first. Any opinion or comments are more than welcome!

TF

Labels (3)
0 Kudos
Reply
1 Reply

1,197 Views
jimmychan
NXP TechSupport
NXP TechSupport

For i.MX6, you should select 7. MX6-based (ARCH_MX6) (NEW)

0 Kudos
Reply