Android SGTL5000 Audio codec setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android SGTL5000 Audio codec setting

3,009件の閲覧回数
ispark
Contributor I

I uses KitKat 4.4.2. i.mx6SL.

default Audio codec configuration can't use HP output.

so I use below setting to command shell.

tinymix 25 on

tinymix 4 127

Then I want to add above command to initialization table init.freescale.rc but no effect.

So question is where should I add user command?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,433件の閲覧回数
ispark
Contributor I

Thanks. I added to original init.rc  and now works.

0 件の賞賛
返信

2,433件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

you may take hardware/imx/alsa/config_wm8962.h and tinyalsa_hal.c for reference.

0 件の賞賛
返信

2,433件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Why don't you modify the audio HAL instead to set those values for you. This is the proper to set such setting.

Regards,

Gary

0 件の賞賛
返信