Android Prebuilt image for sabreauto board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Prebuilt image for sabreauto board

3,544件の閲覧回数
sachusanal
Contributor III

Dear Sir ,

Could you please give me prebuilt android lolipop image for sabreauto board.

and MFGTool for flashing it to sabreauto evaluation kit

please help me

Regards

Sachu

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,075件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

please use mfg tools script mfgtool2-android-mx6q-sabreauto-sdcard.vbs

and images:

Board Support Packages (27)

IMX6-L500-100-ANDROID-DEMO-SD-BSP (REV L5.0.0_1.0.0)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, and i.MX 6Solo Android L5.0.0_1.0.0 BSP

IMX6-L500-100-ANDROID-DEMO-iMX6SX-BSP (REV L5.0.0_1.0.0)

i.MX 6SoloX Android L5.0.0_1.0.0 BSP Binary Demo Files.

Programmers (Flash, etc.) (7)

IMX-L5.0.0-MFG-TOOL (REV L5.0.0_1.0.0)

i.MX 6Family Manufacturing Toolkit for L5.0.0_1.0.0

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,075件の閲覧回数
sachusanal
Contributor III

Dear  Igor,

Thanks for your response.But I couldn't  find out the  IMX6-L500-100-ANDROID-DEMO-SD-BSP (REV L5.0.0_1.0.0)  could you please give me the exact link.

0 件の賞賛
返信

3,075件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,075件の閲覧回数
sachusanal
Contributor III

hai  Igor ,

I downloaded android demo-SD-BSP from the above site. and MFG tool from the(android_L5.0.0_1.0.0-ga_tools ) NXP site.

I extracted the android_L5.0.0_1.0.0-ga_full_image_6qsabreauto image and put the images as per the android user guide steps.

I Copied  following files from either release_package/android_L5.0.0_1.0.0-ga_core_image_6qsabreauto.tar.gz or

release_package/android_L5.0.0_1.0.0-ga_full_image_6qsabreauto.tar.gz to the MFGTool-Dir/Profiles/Linux/OS

Firmware/files/android/sabreauto path.

• u-boot-imx6q.imx

• SD/boot-imx6q.img

• SD/system.img

• SD/recovery.img

Change SABRE-AI S3 (boot mode) to 0101 (from 1-4 bit) to enter download mode.

Power on the board. Using USB cable on the SABRE-AI OTG port, connect a computer running Windows OS to the SABRE-AI board.

flashing by using this vb file  mfgtool2-android-mx6q-sabreauto-nand.vbs .

but i get an error like this . please help me to solve this issue.

    pastedImage_2.png

0 件の賞賛
返信

3,075件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

had you installed NAND to socket, NAND FLASH is not included with shipped boards.

Best regards

igor

0 件の賞賛
返信

3,075件の閲覧回数
sachusanal
Contributor III

Dear Igor ,

I am not installing NAND  on the Socket. is it possible to  install Sd card on the SD socket and flash  mfgtool2-android-mx6q-sabreauto-sdcard.vbs script file.

0 件の賞賛
返信

3,075件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

yes, possible.

Best regards

igor

0 件の賞賛
返信