Android Patch Error: M6.0.1_2.1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Patch Error: M6.0.1_2.1.0

1,521 次查看
bhaveshmoradiya
Contributor II

Hi,

I am trying to build Android M6 For my i.Mx6qp Sabre SD board. I followed the instruction avail in Android 6 documents (Android User's Guid Rev. M6.0.1_1.0.0, 04/2016).

Downloaded release package: android_M6.0.1_2.1.0_source.tar.gz

Getting Android Source code: 

http://storage.googleapis.com/git-repo-downloads/repo

https://android.googlesource.com/platform/menifest/+/refs/heads -b android-6.0.1_r3

git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

git checkout m6.0.1_2.1.0-ga 

clone git://git.freescale.com/imx/uboot-imx.git uboot-imx

git checkout m6.0.1_2.1.0-ga

Patch:

source /opt/android_M6.0.1_2.1.0_source/code/M6.0.1_2.1.0/and_patch.sh

c_patch /opt/android_M6.0.1_2.1.0_source/code/M6.0.1_2.1.0/ imx_M6.0.1_2.1.0

After Few checking I got the following Error:

fatal: bad object f7cfc2cca15736862e45ebef54776e0dfdffeb16
Error! Base version commit f7cfc2cca15736862e45ebef54776e0dfdffeb16 doesn't exist in git /home/<user>/myandroid/prebuilts/qemu-kernel. Stop

Please Help Me I already Spend Too much time on this to solve this error Even I tried with Different version of source file with M6.0.1_1.0.0. But Same Result.

How to Fix This ?

Thanks

标签 (2)
0 项奖励
回复
1 回复

1,052 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bhavesh Moradiya,

The patches need to match the commit version exactly for them to be applied correctly.

In the case of the M6.0.1_2.1.0 you can see the required commit on the Android User’s Guide from this Android BSP. In this case it would be:

$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-6.0.1_r22

Please give it a try. I hope this helps!

Regards,

0 项奖励
回复