Android P build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android P build error

1,859 Views
aravinthkumarja
Senior Contributor II

I'm getting below build error:

 

[ 4% 1361/28756] //hardware/interfaces/bluetooth/audio/2.0:[email protected] header-abi-linker [email protected]
FAILED: out/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]/android_arm_armv8-a_cortex-a53_vendor_shared/[email protected]
prebuilts/clang-tools/linux-x86/bin/header-abi-linker -o 'out/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]/android_arm_armv8-a_cortex-a53_vendor_shared/[email protected]' -so out/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]/android_arm_armv8-a_cortex-a53_vendor_shared/[email protected] -arch arm -Isystem/libhidl/base/include -Isystem/core/libcutils/include_vndk -Isystem/core/libprocessgroup/include -Isystem/core/libutils/include -Isystem/core/libbacktrace/include -Isystem/core/liblog/include_vndk -Isystem/core/libsystem/include -Isystem/libhidl/transport/include -Iout/soong/.intermediates/system/libhidl/transport/manager/1.0/[email protected]_genc++_headers/gen -Iout/soong/.intermediates/system/libhidl/transport/manager/1.1/[email protected]_genc++_headers/gen -Iout/soong/.intermediates/system/libhidl/transport/manager/1.2/[email protected]_genc++_headers/gen -Iout/soong/.intermediates/system/libhidl/transport/base/1.0/[email protected]_genc++_headers/gen -Isystem/libhwbinder/include -Isystem/core/base/include -Iout/soong/.intermediates/system/libhidl/transport/safe_union/1.0/[email protected]_genc++_headers/gen -Iout/soong/.intermediates/hardware/interfaces/audio/common/5.0/[email protected]_genc++_headers/gen -Iout/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]_genc++_headers/gen @'out/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]/android_arm_armv8-a_cortex-a53_vendor_shared/[email protected]'.rsp
Failed to parse the shared library (.so file): out/soong/.intermediates/hardware/interfaces/bluetooth/audio/2.0/[email protected]/android_arm_armv8-a_cortex-a53_vendor_shared/[email protected]
Failed to link and dump elements

0 Kudos
Reply
1 Reply

1,853 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Did you set correct toolchain?

0 Kudos
Reply