Android Naugat Error while doing make

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Naugat Error while doing make

5,371 Views
susangracerapak
Contributor II

Hi,

 I have downloaded the Android Naugat source code and followed the steps present in the User guide. I did ~/bin/repo sync successfully.

While doing  "make systemimage BUILD_TARGET_DEVICE=sd",I am getting the following error.


ERROR: /home/test/myandroid/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/VideoPlayer.java:428: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/test/myandroid/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/VideoPlayer.java:458: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/test/myandroid/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/HdmiApplication.java:328: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/test/myandroid/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/HdmiApplication.java:342: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ninja: build stopped: subcommand failed.
build/core/ninja.mk:148: recipe for target 'ninja_wrapper' failed
make: *** [ninja_wrapper] Error 1

#### make failed to build some targets (23 seconds) ####

 

Could anyone please help me to fix this issue?

Thanks in Advance.

Regards
Susan

0 Kudos
Reply
7 Replies

4,187 Views
Sun1z
Contributor III

Well, I followed the guide of AN11690 (NXP NCI Android Porting Guidelines) and there is a command of "repo sync --force-sync",  which removes all patchs from M6.0.1_2.1.0_GA and caused this issue

0 Kudos
Reply

4,187 Views
Sun1z
Contributor III

I was encountered this issue too, although I use android marshmallow 6.0.1, strange that no any tip on google, any one can give me some advice?

the error log is:

... ...
including ./tools/external/fat32lib/Android.mk ...
No private recovery resources for TARGET_DEVICE sabresd_6dq
Copy: out/target/product/sabresd_6dq/root/fstab.freescale
Building with Jack: out/target/common/obj/APPS/CactusPlayer_intermediates/with-local/classes.dex
Launching background server java -Dfile.encoding=UTF-8 -Xms2560m -XX:+TieredCompilation -jar out/host/linux-x86/framework/jack-launcher.jar -cp out/host/linux-x86/framework/jack.jar com.android.jack.server.JackSimpleServer
ERROR: /home/pvd/i.MX6/android/aosp/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/VideoPlayer.java:428: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/pvd/i.MX6/android/aosp/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/VideoPlayer.java:458: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/pvd/i.MX6/android/aosp/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/HdmiApplication.java:328: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
ERROR: /home/pvd/i.MX6/android/aosp/external/fsl_imx_omx/CactusPlayer/src/com/freescale/cactusplayer/HdmiApplication.java:342: ACTION_WIFI_DISPLAY_DISCONNECTION cannot be resolved or is not a field
make: *** [out/target/common/obj/APPS/CactusPlayer_intermediates/with-local/classes.dex] Error 41

[0;31m#### make failed to build some targets (02:01 (mm:ss)) #### [00m

B.R.

Sun

0 Kudos
Reply

4,187 Views
susangracerapak
Contributor II

Hi Sun,

Try installing all the dependencies again and do repo sync. 

Regards

Susan

0 Kudos
Reply

4,187 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Try installing the bellow libraries and see if that solve your problem:

$ sudo apt-get install libcurl4-openssl-dev nss-updatedb.

Best Regards,

Diego.

0 Kudos
Reply

4,187 Views
Sun1z
Contributor III

Hi Diego,

I have installed libcurl4-openssl-dev and nss-updatedb but got the same error still.

Everything is OK before I ported a NFC driver followed AN11690 (NXP NCI Android Porting Guidelines, 3.2 Android Mashmallow), when the error encountered, I have tried "make update-api" and "make clean" but also the same error.

B. R.

Sun

0 Kudos
Reply

4,187 Views
diegoadrian
NXP Employee
NXP Employee

Let me install the drivers and see if I get the same error as you.

Best regards,

Diego

0 Kudos
Reply

4,187 Views
sachinshah
Contributor I

Hi Support-team,

I am also facing this same issue,could you please help me to resolve this issue.

Thanks in advance

Sachin

0 Kudos
Reply