Android M6 build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android M6 build error

3,288 Views
namratanalawade
Contributor I

Hi All,

I'm building the android source code. I have downloaded the entire packages as mentioned in the Rev. M6.0.1_2.1.0, 07/2016. repo sync is successful, after that we when I try to build the android images, it gives the error as below - 

Internal compiler error (version 1.1-mr2 'Brest' (175100 000a2f91edbe638090dc577801ba49592229fd8b)).
Warning: This may have produced partial or corrupted output.
make: *** [out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex] Error 41
How can I resolve this error ?  attached the snapshot of the error.
Any help would be highly appreciated.
Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

3,030 Views
weirong
Contributor I

hello Namrate:

   I have the same question ,I follows the document android_M6.0.1_2.1.0_docs ,Android_User's_Guide.pdf ,I installed openjdk-7-jdK used sudo apt-get install openjdk-7-jdK command.,but the error is still there.Do you have any propose.

Best regards.

0 Kudos
Reply

3,030 Views
diegoadrian
NXP Employee
NXP Employee

Hello Namrata,

Thank you for writing.

Did you installed openJDK 1.7, or openJDK1.8?

Best regards,

Diego.

0 Kudos
Reply