Android M6 build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android M6 build error

2,195 次查看
namratanalawade
Contributor I

Hi All,

I'm building the android source code. I have downloaded the entire packages as mentioned in the Rev. M6.0.1_2.1.0, 07/2016. repo sync is successful, after that we when I try to build the android images, it gives the error as below - 

Internal compiler error (version 1.1-mr2 'Brest' (175100 000a2f91edbe638090dc577801ba49592229fd8b)).
Warning: This may have produced partial or corrupted output.
make: *** [out/target/common/obj/JAVA_LIBRARIES/framework_intermediates/with-local/classes.dex] Error 41
How can I resolve this error ?  attached the snapshot of the error.
Any help would be highly appreciated.
标签 (2)
标记 (1)
0 项奖励
回复
2 回复数

1,937 次查看
weirong
Contributor I

hello Namrate:

   I have the same question ,I follows the document android_M6.0.1_2.1.0_docs ,Android_User's_Guide.pdf ,I installed openjdk-7-jdK used sudo apt-get install openjdk-7-jdK command.,but the error is still there.Do you have any propose.

Best regards.

0 项奖励
回复

1,937 次查看
diegoadrian
NXP Employee
NXP Employee

Hello Namrata,

Thank you for writing.

Did you installed openJDK 1.7, or openJDK1.8?

Best regards,

Diego.

0 项奖励
回复