Android LL GPIO export automatically at startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android LL GPIO export automatically at startup

3,366 次查看
kamilbystryk
Contributor III

How can I set automatically export and change direction of GPIO at start Android (5.0.2). I want to avoid the need to manual entering:

echo 140 > /sys/class/gpio/export

echo out > /sys/class/gpio/gpio140/direction

commands in root console.

标签 (2)
0 项奖励
回复
2 回复数

2,540 次查看
kamilbystryk
Contributor III

Problem solved - by mistake I put code in wrong section of init.rc:

write /sys/class/gpio/export 142

write /sys/class/gpio/gpio142/direction out

chmod 777 /sys/class/gpio/gpio142/value

0 项奖励
回复

2,540 次查看
jerry2
Contributor II

Hello,

In which section did you insert these commands in the init.rc?

on boot?

0 项奖励
回复