About Encoding On IMX8qm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Encoding On IMX8qm

1,520件の閲覧回数
fengyang
Contributor II

    I need help about video encoding and decoding on imx8qm.

 

On the development board, I found the source code mxc_v4l2_vpu_test, which reads the v4l2 camera image and encodes it and saves it to a local file.I adjusted the code, followed by the imx6 codec routine in mxc_vpu_enc.c to add UDP transmission implementation, and finally using imx8qm as the encoding end, imx6 as the decoding end, Data transmission through udp, but currently encountered some problems: the decoding terminal received the image has a delay of about 3 seconds, i found that imx8qm will have a storage frame operation before encoding, The vpu start encode when the cache area after four frame data , but I think 4 frame data is also not been such a long delay. 

 

If you have ideas or related information about encoding on the IMX8qm,please share to me!

 

Thank you!

0 件の賞賛
返信
1 返信

1,460件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi y

one can look at below link with similar issue and try to use suggested hints

https://community.nxp.com/message/358922#358922 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信