Android L5.1.1 IMX 6 core source patch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android L5.1.1 IMX 6 core source patch

Jump to solution
5,851 Views
duraiselvakumar
Contributor II

Hi,

I'm trying to download Android L5.1.1 source code patch using below link.

Android L5.1.1_2.1.0 GA Release Announcement 

android_L5.1.1_2.1.0-ga_core_source.tar.gz

But can't find the valid link. Could anyone help me to get this code?

Thanks in Advance

Best Regards,

Durai Selvakumar

Android L5.1.1_2.1.0 GA Release Announcementandroidimx6s#imx 6

Labels (3)
Tags (1)
1 Solution
5,139 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can download the IMX6_L5.1.1_2.1.0_ANDROID_SOURCE_BSP here

https://www.nxp.com/webapp/sps/download/preDownload.jsp
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

9 Replies
5,140 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can download the IMX6_L5.1.1_2.1.0_ANDROID_SOURCE_BSP here

https://www.nxp.com/webapp/sps/download/preDownload.jsp
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,139 Views
jhhong
Contributor II

Hi,Rita

About the IMX6_L5.1.1_2.1.0_ANDROID_SOURCE_BSP,we also get the valid link. Could you help me to get this code?

0 Kudos
Reply
5,139 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I share it with you via pan,

Link : https://pan.baidu.com/s/1FDr7Ii7BnqSOTOt_SW8Bjw

Password: i3j1

Have a great day,
Rita

0 Kudos
Reply
5,139 Views
晓锋潘
Contributor I

你好, 我从你分享的百度网盘下载了android_L5.1.1_2.1.0-ga_core_source.tar.gz, 但是打完patch后, kernel中缺少imx_v7_android_defconfig文件, dts目录下也没有sabresd_6dq相关的dts文件, uboot中也没有sabresd_6dq相关的dts文件,

pastedImage_1.png

pastedImage_2.png请问这个怎么解决? 是不是我哪里做的不对?

0 Kudos
Reply
5,140 Views
jhhong
Contributor II

Hi,Rita

      How to download the extended features code packages as follow.Thanks!

android_L5.1.1_2.1.0-ga_omxplayer_source.tar.gz

android_L5.1.1_2.1.0-ga_wfdsink_source.tar.gz

pastedImage_1.png

0 Kudos
Reply
5,140 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About the android_L5.0.0_1.0.0-ga_wfdsink_source.tar.gz and android_L5.1.1_2.1.0-ga_omxplayer_source.tar.gz , they are extended features code package provided by freescale. Not released to public, so if you need it, you'd better to contact the local FAE or Distributor or or Marketing.

Have a nice day

Rita

0 Kudos
Reply
5,140 Views
jhhong
Contributor II

Hi,Rita

      Thanks for your prompt reply!

0 Kudos
Reply
5,140 Views
jhhong
Contributor II

Hi,Rita

Thank you very much!

0 Kudos
Reply
5,140 Views
duraiselvakumar
Contributor II

Hi Rita,

Thanks a lot.

If possible please let me know, whether this source has google's DRM(Widewine DRM) integrated along with this source code patch ?

Best Regards,

Durai Selvakumar

0 Kudos
Reply