Android KitKat touch misaligned, yres_virtual wrong

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android KitKat touch misaligned, yres_virtual wrong

3,529件の閲覧回数
mukelarvin
Contributor IV

Hi,

My touchscreen isn't working quite right. The touch is being reported incorrectly on the Y axis. I noticed the following lines in Logcat.

W/imx6.gralloc( 2101): 32bpp setting of Framebuffer catched!

W/imx6.gralloc( 2101): using (fd=15)

W/imx6.gralloc( 2101): id           = DISP3 BG

W/imx6.gralloc( 2101): xres         = 480 px

W/imx6.gralloc( 2101): yres         = 800 px

W/imx6.gralloc( 2101): xres_virtual = 480 px

W/imx6.gralloc( 2101): yres_virtual = 2688 px

W/imx6.gralloc( 2101): bpp          = 32

W/imx6.gralloc( 2101): r            =  0:8

W/imx6.gralloc( 2101): g            =  8:8

W/imx6.gralloc( 2101): b            = 16:8

W/imx6.gralloc( 2101): width        = 76 mm (160.421051 dpi)

W/imx6.gralloc( 2101): height       = 127 mm (160.000000 dpi)

W/imx6.gralloc( 2101): refresh rate = 65.20 Hz

This may be the source of my problem. Does anyone know where this value is originally being computed? Is it in the graphics driver or in the touchscreen driver (Goodix GT968)?

ラベル(4)
0 件の賞賛
返信
5 返答(返信)

2,904件の閲覧回数
jansirani
Contributor III

Hai all,

   we are having a display with touch IC as GT911.

we required the GT911 drivers to add support to the Android Kitkat 4.4.2  in iMX6SL.

0 件の賞賛
返信

2,904件の閲覧回数
mukelarvin
Contributor IV

Alright I think I may be on the wrong trail. According to this page http://www.phonesdevelopers.com/1721566/ the yres_virtual is deliberately larger than the yres.

"Based on the initialization process EGLDisplaySurface if the framebuffer yres_virtual is greater than yres then framebuffer directly used for double buffering;"


My finger location/pointer location mismatch may be a problem in my touch IC calibration array.

2,904件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Luke,

Were you able to check your IC calibration?, I believe the problem is there...

0 件の賞賛
返信

2,904件の閲覧回数
mukelarvin
Contributor IV

I have sent a sample of my board and screen to the touch screen supplier for calibration. Hopefully that will solve it.

0 件の賞賛
返信

2,904件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Keep us posted on this please!

0 件の賞賛
返信