Android JB not wakeup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android JB not wakeup

3,076 Views
chenhoa
Contributor I

Hi all, I am now porting the Android JB to our customize board using IMX6Q, but it's stop here:

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:01 UTC (1)

Freeing init memory: 240K

init: no such service 'bootanim'

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

UV

  ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: HDMI is not ready!

asoc: can't open platform imx-hdmi-soc-audio.0

warning: `zygote' uses 32-bit capabilities (legacy support in use)

request_suspend_state: wakeup (3->0) at 64456929342 (1970-01-02 00:00:02.115283333 UTC)

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:00, irq=-1)

ADDRCONF(NETDEV_UP): eth0: link is not ready

acc_open

acc_release

ehci_fsl_bus_resume begins, DR

mtp_open

request_suspend_state: sleep (0->3) at 78490105010 (1970-01-02 00:00:16.148458668 UTC)

UV

  UV

    US 921600

I have try with uart or rtc wakeup, but the it still sleep:

echo enabled > /sys/devices/platform/imx-uart.2/tty/ttymxc2/power/wakeup

echo +3 > /sys/class/rtc/rtc0/wakealarm


So, how can I wakeup my Android JB?

Thanks

Labels (2)
0 Kudos
Reply
4 Replies

2,459 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, chen

     Can you measure the PMIC_STBY_REQ pin on the board, better to monitor it from RUN mode->Sleep->wakeup, the level should be low->high->low. If it is high when it is not waking up, that means system still in sleep mode, the wakeup source on your board did NOT work. Please measure this signal first.

0 Kudos
Reply

2,459 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chen,

The board is designed by customs, and which BSP are you use? Would you please attach the whole log file?

Best Regards

Dan

0 Kudos
Reply

2,459 Views
chenhoa
Contributor I

Hi Dan,

Thanks for your reply.

Sorry about my late reply. I just used BSP from Freescale with some modifications to test. I attached the log file

Best regards.

0 Kudos
Reply

2,459 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chen,

I wonder if your problem have solved. If not, which version android BSP are you using? And what have you modified? From the information you gave, it's hard to detect where the problem is?

Best Regards

Dan

0 Kudos
Reply