Android Image on USB Flash for i.MX6 Android 6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android Image on USB Flash for i.MX6 Android 6

1,208 次查看
cxbere
Contributor I

Hello Everyone,

I have a custom board which is designed based i.MX6dl. In my system, first u-boot is loaded from a SPI Flash and then all other Ramdisk, Android System images are loaded eMMC or SD card. It is working very well now. But I need to load Ramdisk, System Image from USB stick.

I mean that, I want to use flash memory instead of SD card or eMMC. I have searched flastboot, but I can't use a PC from OTG, my device is working standalone and using a PC is very hard to update image in industrial environment.

Best Regards,

Ercüment TÜRK

标记 (4)
0 项奖励
回复
1 回复

985 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ercüment

unfortunately such configuration is not provided (not supported) by nxp

in its android releases described on official i.MX software link

i.MX Software|NXP 

one can apply to Professional Services for developing that custom solution

NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复