Android 9 USB pendrive not detected in system level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 9 USB pendrive not detected in system level

2,260件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi All,

I'm using Android 9 in imx6 board. 

I'm using USB H1 and defined in fstab.freescale. 

/devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1* auto auto defaults voldmanaged=usb:auto

 

After boot If I insert pendrive its detected under /dev/block/sda1 

But it not showing inside  /dev/block/vold/ .   

So its not auto mounting also.

 

Can you please help to fix it.

 

Regards,

Aravinth

0 件の賞賛
返信
2 返答(返信)

2,225件の閲覧回数
Aravinthkumar
Contributor III

Hi,

We have fixed the issue.

 

Thank you.

0 件の賞賛
返信

2,237件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you please share which i.MX6 are you using?
is it a custom board or an NXP board?
If possible, could you share the full logs?

Also, please remember that if you're using i.MX6 SABRE Board the only USB supported should be the OTG one, and it is already defined at fstab.freescale:

/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0*  auto auto defaults voldmanaged=usb:auto

Best regards,
Aldo.

0 件の賞賛
返信