[Android 5.0.2] The RTC function is fail.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Android 5.0.2] The RTC function is fail.

Jump to solution
4,560 Views
charleshuang
Senior Contributor II

Hi Freescale

We test the RTC function in Android 5.0.2 version on Demo board.

We tried to change the time.

After system reboot,the time is default value.

The RTC function is fail in Android 5.0.2.

But we try to send command,the RTC function is pass.

example:

# busybox date 2015.10.16-10:41:26

# busybox hwclock -w

# busybox hwclock

Do you have any advice?

Labels (4)
0 Kudos
Reply
1 Solution
4,163 Views
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

View solution in original post

0 Kudos
Reply
6 Replies
4,163 Views
eric-system
Contributor I

Hi All, 

I also met the problem which RTC seeing failed in Android 5.1, does anyone can tell me solution for this issue

Thanks a lot.

Eric

0 Kudos
Reply
4,163 Views
richardmlewis
Contributor I
0 Kudos
Reply
4,163 Views
charleshuang
Senior Contributor II

Hi Kamil Bystryk

I already found the solution and fixed the issue for RTC settting.  Thanks

0 Kudos
Reply
4,163 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi charleshuang,

Would you be nice enough to share your solution? It would be very appreciated and helpful.

Best Regards,

Alejandro

0 Kudos
Reply
4,163 Views
kamilbystryk
Contributor III

OK, but - can You help me with this problem? I try to resolve the same error. Thanks.

0 Kudos
Reply
4,164 Views
kamilbystryk
Contributor III

Charles, did You found solution for RTC settings problem? I see it marked as resolved on.

0 Kudos
Reply