[Android 5.0.2] The 3G function is fail in imx6.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Android 5.0.2] The 3G function is fail in imx6.

878 Views
charleshuang
Senior Contributor II

Hi Freescale

We tried to enable 3G module function in imx6.

Our 3G module is U6300.

I tried to merge (U6300-Android 4.2 version HAL layer) to Android 5.0.

Step1:

When the system boot up in Android, I can get the information in Setting/About tablet/Status.    (include Signal strength ,cellular network type , Service state ,IMEI …… )

Step2:

I  tried to link and setting APN.  Then system reboot.

( debug message will show option1 ttyUSB2: option_instat_callback: error -2 )

I tried to setting Airplane mode is enable.

I send command "pppd connect 'chat -v -s -t 10 "" "AT" "" "ATDT*99#" "CONNECT" ""' user username password password /dev/ttyUSB2 460800 nodetach crtscts debug usepeerdns defaultroute &"in debug console.

I can get ip address and ping google web is pass.

Do you have any advice about 3G function?

Labels (2)
0 Kudos
Reply
1 Reply

639 Views
charleshuang
Senior Contributor II

Hi Freescale

I already porting 3G module with module company.

But I still cannot link google website.

I can get the device ip address from 3G.

Then I ping google dns is pass.

  -->  Ping 8.8.8.8

Please open the attachment file about log message.

But the 3G is not connected correctly.

The Exclamation Point Icon on Cellular Data Icon.

When I open browser, I cannot open google or any website.

Do you have any example porting 3G module in Android 5.0.0?

Or do you have success example porting 3G module in imx6 Android 5.0.0?

Thanks

0 Kudos
Reply