Android 4.2.2 Second Screen with i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 4.2.2 Second Screen with i.MX6

1,210 Views
vukasinristic
Contributor I

Hi,

I need to have Android Second Screen in full HD resolution. I have an issue when first screen is smaller then second. Overscan is used but the resolution is the same as on primary LCD monitor. However, external monitor have normal picture over the whole screen but with much lower resolution.

If I use HD monitor as primary screen, everything works well, but that isn't my use case. Android applications always use secondary screen for presentation view.

I have an idea to set kernel frame buffer parameters as I have two monitors with HD resolution and than scale first to LCD resolution. Is it could be done form android SurfaceFlinger service?

Please suggest me some solution or/and solution details.

I use Android 4.2.2 BSP with kernel  3.0.35

Best, Vukasin

Labels (3)
0 Kudos
Reply
1 Reply

1,011 Views
gusarambula
NXP TechSupport
NXP TechSupport

SergioSolis, perhaps you may be able to provide a comments on this?

0 Kudos
Reply