Andorid7.1.2 preempt error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Andorid7.1.2 preempt error

1,377 Views
1483887104
Contributor I

Andorid 7.1.2

kernel: 4.9.17-g6c73f61-dirty

[ 10.132165] ------------[ cut here ]------------
[ 10.136993] WARNING: CPU: 0 PID: 261 at kernel/sched/core.c:3346 _raw_spin_unlock+0x24/0x50
[ 10.190694] DEBUG_LOCKS_WARN_ON(val > preempt_count())
[ 10.195727] Modules linked in:
[ 10.198821] CPU: 0 PID: 261 Comm: healthd Not tainted 4.9.17-g6c73f61-dirty #75
[ 10.206148] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 10.206189] [<c0110e4c>] (unwind_backtrace) from [<c010ca80>] (show_stack+0x10/0x14)
[ 10.206210] [<c010ca80>] (show_stack) from [<c0c76178>] (dump_stack+0x80/0x94)
[ 10.206227] [<c0c76178>] (dump_stack) from [<c01350a4>] (__warn+0xec/0x104)
[ 10.206240] [<c01350a4>] (__warn) from [<c0135104>] (warn_slowpath_fmt+0x48/0x6c)
[ 10.206259] [<c0135104>] (warn_slowpath_fmt) from [<c0c81d58>] (_raw_spin_unlock+0x24/0x50)
[ 10.206282] [<c0c81d58>] (_raw_spin_unlock) from [<c02c37a8>] (SyS_timerfd_settime+0x170/0x53c)
[ 10.206302] [<c02c37a8>] (SyS_timerfd_settime) from [<c0107e00>] (ret_fast_syscall+0x0/0x3c)
[ 10.279650] ---(func:prp_enc_select)---,Line:523.
[ 10.279880] ---(func:prp_enc_select)---,Line:523.
[ 10.285125] ---[ end trace 58886388809caaa7 ]---
[ 10.285795] healthd: No battery devices found

How to fix this problem?

Thanks a lot.

Labels (1)
0 Kudos
Reply
1 Reply

1,266 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please share with us the complete output log file?

Furthermore, can you please share the steps that you followed to build the image?

Best Regards,

Diego.

0 Kudos
Reply