Andorid7.1.2 preempt error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Andorid7.1.2 preempt error

1,383件の閲覧回数
1483887104
Contributor I

Andorid 7.1.2

kernel: 4.9.17-g6c73f61-dirty

[ 10.132165] ------------[ cut here ]------------
[ 10.136993] WARNING: CPU: 0 PID: 261 at kernel/sched/core.c:3346 _raw_spin_unlock+0x24/0x50
[ 10.190694] DEBUG_LOCKS_WARN_ON(val > preempt_count())
[ 10.195727] Modules linked in:
[ 10.198821] CPU: 0 PID: 261 Comm: healthd Not tainted 4.9.17-g6c73f61-dirty #75
[ 10.206148] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 10.206189] [<c0110e4c>] (unwind_backtrace) from [<c010ca80>] (show_stack+0x10/0x14)
[ 10.206210] [<c010ca80>] (show_stack) from [<c0c76178>] (dump_stack+0x80/0x94)
[ 10.206227] [<c0c76178>] (dump_stack) from [<c01350a4>] (__warn+0xec/0x104)
[ 10.206240] [<c01350a4>] (__warn) from [<c0135104>] (warn_slowpath_fmt+0x48/0x6c)
[ 10.206259] [<c0135104>] (warn_slowpath_fmt) from [<c0c81d58>] (_raw_spin_unlock+0x24/0x50)
[ 10.206282] [<c0c81d58>] (_raw_spin_unlock) from [<c02c37a8>] (SyS_timerfd_settime+0x170/0x53c)
[ 10.206302] [<c02c37a8>] (SyS_timerfd_settime) from [<c0107e00>] (ret_fast_syscall+0x0/0x3c)
[ 10.279650] ---(func:prp_enc_select)---,Line:523.
[ 10.279880] ---(func:prp_enc_select)---,Line:523.
[ 10.285125] ---[ end trace 58886388809caaa7 ]---
[ 10.285795] healthd: No battery devices found

How to fix this problem?

Thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 返信

1,272件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please share with us the complete output log file?

Furthermore, can you please share the steps that you followed to build the image?

Best Regards,

Diego.

0 件の賞賛
返信