Analog Camera with M4 Core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Analog Camera with M4 Core

2,064件の閲覧回数
burakdinc
Contributor I

Hi,
I'm working on IMX6 SoloX. When the Board is energized I need to control an Analog Camera with M4 as soon as possible (before Android initialize completed). For M4 Core, I'm using "FreeRTOS IMX6 SoloX". I couldn't find any C library or driver about VADC, CSI, LCDIF and LVDS.
I guess modifying and implementing linux driver files for my application could be an option. Is it possible to modify linux drivers for M4 Core? or should I write all drivers for M4?

If modifying linux drivers for M4 is appropriate, could you please tell me which files should i implement?

ラベル(1)
0 件の賞賛
返信
1 返信

1,956件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi burak

please find attached Linux Manual and Porting Guide with description

of all nxp linux drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信