Amphion Malone encoder and supported pixel formats

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Amphion Malone encoder and supported pixel formats

1,907 Views
crg7475
Contributor III

I know that the Hantro encoder on the i.MX8M Mini supports not only multiple YUV but also multiple RGB formats.

But what about the Amphion Malone encoder on the QuadMax? The kernel driver code indicates that only YUV formats are supported as the encoder input. Is this correct?

If so, I need a suggestion for a solution. I am composing video frames with G2D. G2D can take YUV and RGB as input, but can only output RGB formats. Is there anything on the i.MX8 QuadMax that would be able to convert from YUV to RGB formats? I'd like to avoid CPU-based format conversions, since these tend to be much slower.

0 Kudos
Reply
3 Replies

1,892 Views
b36401
NXP Employee
NXP Employee

i.MX8M processor series has Hantro VPU and i.MX8 series has Amphion VPU.
However I am aftaid not all formats of are supported with the driver.

0 Kudos
Reply

1,888 Views
crg7475
Contributor III

Alright, thanks. Does the i.MX8 then have some sort of subsystem that could do an RGB->YUV conversion? On the i.MX6, I would have used the IPU for this, but the i.MX8 has no IPU.

0 Kudos
Reply

1,833 Views
b36401
NXP Employee
NXP Employee

ISI (Image Sensor Interface) of i.MX8 processor has color space conversion.

0 Kudos
Reply