Altium Files for i.MX 8M Mini EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Altium Files for i.MX 8M Mini EVK

27,324件の閲覧回数
arun_panangala
Contributor II

Hello,

Is it possible for me get the Altium Design files for 8MMINILPD4-EVK SoM Board. I am unable to convert the Allegro files to Altium from the Data pack provided in the .zip file.

Kind Regards,

Arun

52 返答(返信)

10,090件の閲覧回数
lewismarkwell
Contributor II

Can anyone share the Altium version of i.mx8 Mini EVK with DDR4?
I have contacted support and they have suggested they only have the 8M Nano in Altium available to share.

0 件の賞賛
返信

11,684件の閲覧回数
commsmason
Contributor I

Can I also please get the Altium files for 8MMINILPD4-EVK (SoM & base)

0 件の賞賛
返信

11,672件の閲覧回数
Yuri
NXP Employee
NXP Employee

@commsmason 
Hello,

   Please create separate request.

Regards,
Yuri.

0 件の賞賛
返信

11,390件の閲覧回数
wanglee
Contributor III

CAN you  send  me  the  Altium Files for i.MX 8M Mini EVK?  

0 件の賞賛
返信

11,969件の閲覧回数
bryan_l_courtne
Contributor III

Hi Victor,

Can i get the Altium files for both evaluation boards for the 8M mini.

Thanks

Bryan

0 件の賞賛
返信

11,969件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello Bryan,
I just sent you the link via e-mail.

0 件の賞賛
返信

6,542件の閲覧回数
diegongh9
Contributor I
Hello,
please could you share the Altium version of i.mx8 Mini EVK with DDR4? Impossible to import Allegro files. Thank in advance
0 件の賞賛
返信

11,626件の閲覧回数
q12b
Contributor I

Hi @b36401 , @Yuri 

Can I get the Altium files?

I need the FBGA 14x14mm footprint and model. I cannot convert from Allegro files.

Thanks.

0 件の賞賛
返信

11,619件の閲覧回数
Yuri
NXP Employee
NXP Employee

@q12b 
Hello,

  Please create separate request / thread.

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 件の賞賛
返信

11,969件の閲覧回数
sijiniu-b17591
NXP Employee
NXP Employee

b36401

I also need Altinum files of IMX8M mini LPDDR4/DDR4 evk. Could you send it to me? Thanks.

0 件の賞賛
返信

11,969件の閲覧回数
b36401
NXP Employee
NXP Employee

Kenny,

I sent you the files.


Fred,

Please tell me your email for I can send you the files as well.

0 件の賞賛
返信

11,890件の閲覧回数
JacobSkjoet
Contributor I

Hi b36401,

 

Sorry to pester you, but could you be so kind to send me the Altium design files too..

Best regards

Jacob

0 件の賞賛
返信

11,973件の閲覧回数
sijiniu-b17591
NXP Employee
NXP Employee

b36401‌   Thanks.

[email protected] 

0 件の賞賛
返信

11,973件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello Fred,

I sent you the files as well.

0 件の賞賛
返信

11,973件の閲覧回数
sijiniu-b17591
NXP Employee
NXP Employee

b36401

Got it. Thank you very much.

0 件の賞賛
返信

11,969件の閲覧回数
kenny_wang1
Contributor I

Dear Victor,

 

      Please help to send me  the Altium design files of  8MMINILPD4-CPU (SOM board) and 8MMINI-BB (base board).

        

 

Best Regards,

Kenny

0 件の賞賛
返信

11,969件の閲覧回数
rafb
Contributor I

Dear Victor,

Sorry to ask, but I also would like to receive the files in Altium format of the 8M mini and 8M nano boards.

Many thanks for your help.

Raphael

0 件の賞賛
返信

11,969件の閲覧回数
rausov
Contributor I

Hello Victor,

the files that you shared are an Allegro project, not the Altium ones.

0 件の賞賛
返信

11,969件の閲覧回数
rausov
Contributor I

Hello Victor,

can you send me the altium projects of the i.MX8 boards that you have.

Thank you for your support,

Valerio.

0 件の賞賛
返信

11,969件の閲覧回数
b36401
NXP Employee
NXP Employee

Valerio,
I sent you the files.

0 件の賞賛
返信