Altium Files for i.MX 8M Mini EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Altium Files for i.MX 8M Mini EVK

9,962 Views
arun_panangala
Contributor II

Hello,

Is it possible for me get the Altium Design files for 8MMINILPD4-EVK SoM Board. I am unable to convert the Allegro files to Altium from the Data pack provided in the .zip file.

Kind Regards,

Arun

51 Replies

2,485 Views
lewismarkwell
Contributor II

Can anyone share the Altium version of i.mx8 Mini EVK with DDR4?
I have contacted support and they have suggested they only have the 8M Nano in Altium available to share.

0 Kudos
Reply

4,079 Views
commsmason
Contributor I

Can I also please get the Altium files for 8MMINILPD4-EVK (SoM & base)

0 Kudos
Reply

4,067 Views
Yuri
NXP Employee
NXP Employee

@commsmason 
Hello,

   Please create separate request.

Regards,
Yuri.

0 Kudos
Reply

3,785 Views
wanglee
Contributor III

CAN you  send  me  the  Altium Files for i.MX 8M Mini EVK?  

0 Kudos
Reply

4,364 Views
bryan_l_courtne
Contributor III

Hi Victor,

Can i get the Altium files for both evaluation boards for the 8M mini.

Thanks

Bryan

0 Kudos
Reply

4,364 Views
b36401
NXP Employee
NXP Employee

Hello Bryan,
I just sent you the link via e-mail.

0 Kudos
Reply

4,021 Views
q12b
Contributor I

Hi @b36401 , @Yuri 

Can I get the Altium files?

I need the FBGA 14x14mm footprint and model. I cannot convert from Allegro files.

Thanks.

0 Kudos
Reply

4,014 Views
Yuri
NXP Employee
NXP Employee

@q12b 
Hello,

  Please create separate request / thread.

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 Kudos
Reply

4,364 Views
sijiniu-b17591
NXP Employee
NXP Employee

b36401

I also need Altinum files of IMX8M mini LPDDR4/DDR4 evk. Could you send it to me? Thanks.

0 Kudos
Reply

4,364 Views
b36401
NXP Employee
NXP Employee

Kenny,

I sent you the files.


Fred,

Please tell me your email for I can send you the files as well.

0 Kudos
Reply

4,285 Views
JacobSkjoet
Contributor I

Hi b36401,

 

Sorry to pester you, but could you be so kind to send me the Altium design files too..

Best regards

Jacob

0 Kudos
Reply

4,368 Views
sijiniu-b17591
NXP Employee
NXP Employee

b36401‌   Thanks.

Fred.niu@nxp.com 

0 Kudos
Reply

4,368 Views
b36401
NXP Employee
NXP Employee

Hello Fred,

I sent you the files as well.

0 Kudos
Reply

4,368 Views
sijiniu-b17591
NXP Employee
NXP Employee

b36401

Got it. Thank you very much.

0 Kudos
Reply

4,364 Views
kenny_wang1
Contributor I

Dear Victor,

 

      Please help to send me  the Altium design files of  8MMINILPD4-CPU (SOM board) and 8MMINI-BB (base board).

        

 

Best Regards,

Kenny

0 Kudos
Reply

4,364 Views
rafb
Contributor I

Dear Victor,

Sorry to ask, but I also would like to receive the files in Altium format of the 8M mini and 8M nano boards.

Many thanks for your help.

Raphael

0 Kudos
Reply

4,364 Views
rausov
Contributor I

Hello Victor,

the files that you shared are an Allegro project, not the Altium ones.

0 Kudos
Reply

4,364 Views
rausov
Contributor I

Hello Victor,

can you send me the altium projects of the i.MX8 boards that you have.

Thank you for your support,

Valerio.

0 Kudos
Reply

4,364 Views
b36401
NXP Employee
NXP Employee

Valerio,
I sent you the files.

0 Kudos
Reply

4,364 Views
wdunkley
Contributor III

Victor, I've been trying to get the Orcad files imported into Altium for a week. Could I get the Altium versions of the i.MX 8M Mini Evaluation Kit DDR4 and LPDDR4 SCH and PCB files? Thank you So much for your help.

0 Kudos
Reply