Alsa overrun/underrun errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alsa overrun/underrun errors

5,837 Views
yehudastern
Contributor II

Hi,

I'm using 2 TLV320AIC3106 codecs, connected to SSI1 and SSI2, and I recently changed the sampling rate from 44.1KHz to 48KHz.

When I run alsa loops (see below), I usually get the xrun error message roughly once in every 2 minutes:  overrun!!! (at least xx ms long) or underrun!!! (at least xx ms long).

BTW, before changing the sampling rate, the error messages appeared a lot more often (every couple of seconds).

This problem happens with both codecs, even if the loops are internal for each codec.   Here are the alsa loops I run:

arecord -D hw:0 -f S16_LE -r 48000 -B 8000 -F 1000 -c 2 | aplay -D hw:0 -f S16_LE -r 48000 -B 4000 -F 2000 -c 2run  |

arecord -D hw:1 -f S16_LE -r 48000 -B 8000 -F 1000 -c 2 | aplay -D hw:1 -f S16_LE -r 48000 -B 4000 -F 2000 -c 2

Regards,

Yehuda

Labels (2)
0 Kudos
Reply
1 Reply

4,117 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yehuda

one can check if this behaviour is caused by bus bandwidth limitation

running mmdc profiling tool

https://community.freescale.com/message/481292#comment-481292

If this is bandwidth limitation, then it is necessary to decrease bus loading

removing gpu/vpu applications or change them in such way, so they consume

less bandwidth.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply