Alexa-AVS-Sample i.MX8 WakeWord Install & Licensing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alexa-AVS-Sample i.MX8 WakeWord Install & Licensing

1,809 Views
cesar_hernande1
Contributor II

Hi,

I have compiled and installed the i.mx8 avs-image based on this guide: Build Alexa SDK (AVS) image for i.MX8M EVK board (with Yocto Morty, Kernel4.9) 

I see that the Alexa app works fine but I need to add sensory wakeword

I have acquired the sdk and license from sensory but i have no clue how I need to activate so wakeword will work with my Alexa_AVS_App

My question is how I can do this and also install the license from sensory? Below is a picture of what i get when i try to renew the license and was wondering if anyone can help. Any help is appreciated. Thanks.

pastedImage_2.png

0 Kudos
Reply
1 Reply

1,530 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot help you with this problem. Since we do not support directly the Alexa demo. However, I am aware that the sensory license is not currently supported in the i.MX8MQ for the reason that the libraries were made for a 32 bit processor and the i.MX8MQ is a 64 bit processor. Actually, I think that at the time you are building the image, there is a text where it says what I told you.

I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply