Advanced Toolkit Warning, i.MX vs ColdFire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Advanced Toolkit Warning, i.MX vs ColdFire

ソリューションへジャンプ
2,060件の閲覧回数
TomE
Specialist II

We're using the i.MX53 on a Karo TX53 board.

I managed (with help) to wipe out the RedBoot bootloader, and was then advised to use the "Advanced Toolkit" to reflash the boot.

The installer (possibly a little too old) was the file "FSL_ATK_TOOL_WINS_STD_INSTALL_1_68.exe". I've looked on Freescale's site and there doesn't seem to be anything newer, AND this isn't linked from the i.MX53 page, only the i.MX27.

The installation went and installed some USB Drivers. That's always a sign of problems.


The Toolkit wouldn't work. It couldn't find the i.MX53 at all. The interface implied it might work with a Serial Port or USB (it let me select Serial), but that didn't work either.

Then I found that it had also wrecked my existing installation of the drivers for the P&E Micro USB ColdFire Multilink. They both use something called "Jungo", but they seem to be mutually incompatible.

In the Device Manager on my PC, the "Jungo / USB Multilink 2.0" icon had the yellow triangle next to it.

Luck for me, the "System Restore" was able to put my computer back before the failed install.

Tom

ラベル(3)
0 件の賞賛
返信
1 解決策
1,579件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Tom,

     Advanced Toolkit is also called ATK tool which is used to burn images into flash on board based on i.mx SOC. But this tool has been replaced with MFG Tool , and Freescale will not support and maintence ATK Tool.

     So you will have to use MFG Tool to burn images into flash on i.mx53 board. you can download it from freescale offical website :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...

imx-mfg-tool.png

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,579件の閲覧回数
YixingKong
Senior Contributor IV

Tom

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信
1,580件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Tom,

     Advanced Toolkit is also called ATK tool which is used to burn images into flash on board based on i.mx SOC. But this tool has been replaced with MFG Tool , and Freescale will not support and maintence ATK Tool.

     So you will have to use MFG Tool to burn images into flash on i.mx53 board. you can download it from freescale offical website :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...

imx-mfg-tool.png

Regards,

Weidong

0 件の賞賛
返信