Please take into account two features when considering address decoding :
1. Mapping scheme uses zero address offset and it is assumed that base memory
address of 0x1000_0000 should be added to get real address.
2. When address range of memory is 2G (per CS) low 256 MB memory are not used.
So, total memory available for DDR is 4GB-256MB.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------