Additional Chip Select lines for SPI interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Additional Chip Select lines for SPI interface

1,213件の閲覧回数
harishs
Contributor I

Hi,

We are developing one of our product using CM-FX6  ( IMX6 Quad based COM form Compulab), is it possible to use available GPIO lines for additional Chip select lines for SPI interface required, the dedicated Chip select lines of SPI are used for some other interfaces in our design.

Regards,

Harish.S

ラベル(1)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible to use available GPIO lines for additional Chip select lines for SPI interface.
But users should control these GPIO lins in software.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信