Adding uboot and kernel images into Ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding uboot and kernel images into Ubuntu

2,950 Views
prashant_chopad
Contributor II

Hi,

I referred Ubuntu-i.MX8M.pdf. I used AWS to create Ubuntu BSP.

I can not do "Step-9 replace filesystem" as mentioned in above said PDF, as my SD card is not mountable on AWS.

Now I have folder "ubuntu-rootfs".

Would you please guide me to know how to flash it on my SD card?

How to include/add kernel and ubuntu images into the  folder "ubuntu-rootfs".

Regards,

Prashant

0 Kudos
Reply
4 Replies

2,930 Views
prashant_chopad
Contributor II

Hi,

Followed given steps:

1. Created ubuntu-rootfs.tar.bz2 on AWS server.

2. Downloaded on my Laptop having Ubuntu 18.04 LTS.

3. Connected 16GB SD card over USB to Laptop.

4. Formatted it using # sudo mkfs.ext4 /dev/sda1

5. Went inside the mounted folder : # cd /media/pch/216cfe51-d19e-443c-aea1-5295d81edd21

     # sudo tar -jxvf /home/pch/AWS/ubuntu-rootfs.tar.bz2      

     Also tried it next time with # tar -xvJf ubuntu-rootfs.tar.bz2 -C /dev/sda1

6. Unmounted SD card and inserted on iMX8M Dev board.

7. Adjusted switches SW1101 and SW1102 to boot from MicroSD/SDHC2.

8. USB microB debug port connected to Laptop. Used Putty serial – ttyUSB0 (or 1).

9. Did not get anything on serial.

10. RED PWR LED was ON. Nothing else.

Would you please help me to understand what is going wrong? Why board is not booting up?

Regards,

Prashant

0 Kudos
Reply

2,941 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello prashant,

 

You can burn the sd card with  $sudo dd.

 

Regards

 

0 Kudos
Reply

2,897 Views
prashant_chopad
Contributor II

Hi,

I downloaded prebuilt images : L5.4.24-2.1.0_images_MX8MMEVK.zip

Used *.wic from them on SD card.

Adjusted switches SW1101 and SW1102 to boot from MicroSD/SDHC2.

Connected USB microB debug port to Laptop. Used Putty serial – ttyUSB0 (or 1).

Did not get anything on serial.

RED PWR LED was ON. Nothing else.

What would go wrong?

Regards,

Prashant

0 Kudos
Reply

2,882 Views
prashant_chopad
Contributor II

Used UUU and my board booted.

0 Kudos
Reply