Adding uboot and kernel images into Ubuntu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding uboot and kernel images into Ubuntu

2,203件の閲覧回数
prashant_chopad
Contributor II

Hi,

I referred Ubuntu-i.MX8M.pdf. I used AWS to create Ubuntu BSP.

I can not do "Step-9 replace filesystem" as mentioned in above said PDF, as my SD card is not mountable on AWS.

Now I have folder "ubuntu-rootfs".

Would you please guide me to know how to flash it on my SD card?

How to include/add kernel and ubuntu images into the  folder "ubuntu-rootfs".

Regards,

Prashant

0 件の賞賛
返信
4 返答(返信)

2,183件の閲覧回数
prashant_chopad
Contributor II

Hi,

Followed given steps:

1. Created ubuntu-rootfs.tar.bz2 on AWS server.

2. Downloaded on my Laptop having Ubuntu 18.04 LTS.

3. Connected 16GB SD card over USB to Laptop.

4. Formatted it using # sudo mkfs.ext4 /dev/sda1

5. Went inside the mounted folder : # cd /media/pch/216cfe51-d19e-443c-aea1-5295d81edd21

     # sudo tar -jxvf /home/pch/AWS/ubuntu-rootfs.tar.bz2      

     Also tried it next time with # tar -xvJf ubuntu-rootfs.tar.bz2 -C /dev/sda1

6. Unmounted SD card and inserted on iMX8M Dev board.

7. Adjusted switches SW1101 and SW1102 to boot from MicroSD/SDHC2.

8. USB microB debug port connected to Laptop. Used Putty serial – ttyUSB0 (or 1).

9. Did not get anything on serial.

10. RED PWR LED was ON. Nothing else.

Would you please help me to understand what is going wrong? Why board is not booting up?

Regards,

Prashant

0 件の賞賛
返信

2,194件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello prashant,

 

You can burn the sd card with  $sudo dd.

 

Regards

 

0 件の賞賛
返信

2,150件の閲覧回数
prashant_chopad
Contributor II

Hi,

I downloaded prebuilt images : L5.4.24-2.1.0_images_MX8MMEVK.zip

Used *.wic from them on SD card.

Adjusted switches SW1101 and SW1102 to boot from MicroSD/SDHC2.

Connected USB microB debug port to Laptop. Used Putty serial – ttyUSB0 (or 1).

Did not get anything on serial.

RED PWR LED was ON. Nothing else.

What would go wrong?

Regards,

Prashant

0 件の賞賛
返信

2,135件の閲覧回数
prashant_chopad
Contributor II

Used UUU and my board booted.

0 件の賞賛
返信