Adding serial support to Qt4.6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding serial support to Qt4.6.0

ソリューションへジャンプ
1,796件の閲覧回数
nishad_kamdar
Contributor IV

Hi,

I have a custom iMX6q board and i am using Ltib with L3.0.35_4.1.0 Kernel.

I have installed QT version 4.6.0 and i am successfully able to run simple applications.

However, i specifically need serial connectivity support for my application.

As 4.6.0 does not by default have serial driver support , it would be very helpful if you could suggest the procedure to add serial connectivity support to the QT 4.6.0.

regards,

nishad

ラベル(2)
0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1 返信
1,672件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

This may useful for you.

< QtSerialPort | Qt Wiki | Qt Project >

0 件の賞賛
返信