Adding custom mipi camera for Android (Timeouts)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Adding custom mipi camera for Android (Timeouts)

跳至解决方案
2,695 次查看
dennis3
Contributor V

I have a custom MIPI camera that I've written a driver for.  I've integrated this camera into Linux w/ the Yocto build and can successfully stream and display camera images.

The driver is the same for Android 8.  (Similar kernel version and camera module, DTS is the same.)  In addition, I've followed the guide to customize the init.rc to set the back_camera_name property accordingly to my custom camera and I've created an libcamera3 Camera implementation for my camera in the vendor library.

In Android, when the camera app is launched, I see all the correct dmesg output to suggest our driver and library are successfully called but the actual data fails to stream:

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

I've checked mipi phy status and err1/2 registers and they suggest mipi is streaming as expected.  (Again on Linux at this point the camera can stream images fine.. same hardware/driver).

Can anyone suggest how I might debug further on Android why it is failing to stream? 

Our data format is YUYV (YUV422).  On linux, gstreamer can take this format directly to the IPU and from there we can convert to to a format available for display.  I don't know if the fact that we can't support NV12 is a problem or not on Android or if that would cause the timeout we're seeing.

Here is a snippet of the Android logcat output for the FslCameraHAL layer:

01-01 00:00:15.481   246   246 I FslCameraHAL: Camera fourcc to format code is: 0x14 ->(HAL_PIXEL_FORMAT_YCBCR_422_I)

01-01 00:00:15.481   246   246 I FslCameraHAL: enum frame size w:1920, h:1080

01-01 00:00:15.481   246   246 I FslCameraHAL: SupportedPictureSizes: 1920 x 1080

01-01 00:00:15.481   246   246 I FslCameraHAL: SupportedPreviewSizes: 1920 x 1080

01-01 00:00:15.481   246   246 I FslCameraHAL: FrameDuration is 33331760, 30000000000

01-01 00:00:15.481   246   246 I FslCameraHAL: mMaxWidth:1920, mMaxHeight:1080

01-01 00:00:15.481   246   246 I FslCameraHAL: Thine, mFocalLength:3.370000, mPhysicalWidth:2.772000, mPhysicalHeight 1.512000

01-01 00:05:03.771   246   352 I FslCameraHAL: openDev:0: Opening camera device

01-01 00:05:03.771   246   352 I FslCameraHAL: openDev

01-01 00:05:04.409   246   246 I FslCameraHAL: configureStreams:0: stream_config 0xbeff0430, num 2, streams 0xb3f191d8, mode 0

01-01 00:05:04.409   246   246 I FslCameraHAL: config 0, type 0, res 1920x1080, fmt 0x21, usage 0x3, maxbufs 0, priv 0x0, rotation 0

01-01 00:05:04.409   246   246 I FslCameraHAL: config 1, type 0, res 1920x1080, fmt 0x22, usage 0x100, maxbufs 0, priv 0x0, rotation 0

01-01 00:05:04.409   246   246 I FslCameraHAL: Stream create capture stream

01-01 00:05:04.409   246   246 I FslCameraHAL: stream: w:1920, h:1080, format:0x21, usage:0x20303, buffers:2

01-01 00:05:04.409   246   246 I FslCameraHAL: Stream create preview stream

01-01 00:05:04.409   246   246 I FslCameraHAL: stream: w:1920, h:1080, format:0x0, usage:0x20302, buffers:3

01-01 00:05:04.578   246   352 I FslCameraHAL: constructDefaultRequestSettings:0: type=1

01-01 00:05:04.672   246   246 E FslCameraHAL: configure: invalid stream parameters

01-01 00:05:04.673   246   309 E FslCameraHAL: invalid state:0x201 go into start state

01-01 00:05:14.716   246   309 E FslCameraHAL: onFrameAcquireLocked: VIDIOC_DQBUF Failed

标签 (3)
标记 (4)
0 项奖励
回复
1 解答
2,414 次查看
dennis3
Contributor V

Actually, yes I did verify that.  I was able to get streaming to work by changing the media formats in the libcamera addition for my camera.  I originally put YUYV as the format because that is what our camera can produce.  I since learned the format here (libcamera HAL) isn't necessarily what the camera can produce but also includes what the IPU can produce.  Since the IPU can convert YUYV to NV12 et. al., those are what actually needed listed because Android must have the NV12.

Anyway, at least that's my understanding of the problem.  There may be parts I don't understand correctly or haven't completely implemented but it's working for me at this time.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,414 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you verify if you have access to the camera at kernel level?

Otherwise, it can be due that the application is not recognizing your new hardware. Please see the below guide, probably it could help you:

https://developer.android.com/guide/topics/media/camera

Best regards,

Diego.

0 项奖励
回复
2,415 次查看
dennis3
Contributor V

Actually, yes I did verify that.  I was able to get streaming to work by changing the media formats in the libcamera addition for my camera.  I originally put YUYV as the format because that is what our camera can produce.  I since learned the format here (libcamera HAL) isn't necessarily what the camera can produce but also includes what the IPU can produce.  Since the IPU can convert YUYV to NV12 et. al., those are what actually needed listed because Android must have the NV12.

Anyway, at least that's my understanding of the problem.  There may be parts I don't understand correctly or haven't completely implemented but it's working for me at this time.

0 项奖励
回复