Adding a sensor to Android but HAL doesn't seem to be initialized.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Adding a sensor to Android but HAL doesn't seem to be initialized.

跳至解决方案
12,499 次查看
dennis3
Contributor V

I'm trying to add an Ambient Light Sensor to an imx8mq Android 10 project.

Steps so far:

BoardConfig: 

 + BOARD_USE_SENSOR_FUSION := true

MyBoard.mk

 +PRODUCT_PACKAGES += \
   [email protected] \
   [email protected] \
   sensors.imx8

init.rc

 + added permissions and sys path to my ALS sensor can read lux and set mode.

/vendor/nxp-opensource/imx/libsensors_sensorhub

+ modified LightSensor to be specific to my device

+ modified sensors.cpp to include my ALS sensor in mSensors and SensorList

At run time, I've modified the functions in sensors.cpp to have an ALOGD statement in the various functions.  open_sensors is called and you can see my sensor in pos 0 (the only sensor) has a valid fd.  

08-07 21:01:55.009 3157 3157 I Sensors : open_sensors
08-07 21:01:55.009 3157 3157 I Sensors : sensors_poll_context_t
08-07 21:01:55.504 3157 3157 I Sensors : fillPollFd
08-07 21:01:55.504 3157 3157 I Sensors : mSensors[0].fd = 7

There is also some statements about the service starting up and being registered.

08-07 21:01:55.524 3157 3157 I ServiceManagement: Registered [email protected]::ISensors/default (start delay of 689ms)
08-07 21:01:55.524 3157 3157 I ServiceManagement: Removing namespace from process name [email protected] to [email protected].
08-07 21:01:55.524 3157 3157 I [email protected]: Registration complete for [email protected]::ISensors/default.

However, adb shell:

>dumpsys sensor server

No Sensors on the device
devInitCheck : -19

I noticed also that sensors__get_sensors_list was never called.

So it seems I'm missing some step in the glue between the system service and the hw implementation.  Any suggestions where I might find that?

FWIW, I can go to the sys directory and manually check the device is reporting lux right.  Also 

> getevent -vl /dev/input/event2

0003 0028 0000000b
0000 0000 00000000
0003 0028 00000062
0000 0000 00000000
0003 0028 00000034
0000 0000 00000000
0003 0028 00000062
0000 0000 00000000

The device driver appears to be working correctly and reporting events that are sensitive to when I'm covering up the ALS or not.

标记 (4)
1 解答
12,398 次查看
dennis3
Contributor V

Ok I found the missing step.  Since I started with a board config that had no sensors, the vendor manifest didn't include the HAL entry for the sensors.

in /vendor/etc/vintf/manifest.xml

+ <hal format="hidl">
+ <name>android.hardware.sensors</name>
+ <transport>hwbinder</transport>
+ <version>1.0</version>
+ <interface>
+ <name>ISensors</name>
+ <instance>default</instance>
+ </interface>
+ </hal>

After adding that, the HAL layer properly communicates the sensors to Android and the light sensor is now available:

在原帖中查看解决方案

3 回复数
12,399 次查看
dennis3
Contributor V

Ok I found the missing step.  Since I started with a board config that had no sensors, the vendor manifest didn't include the HAL entry for the sensors.

in /vendor/etc/vintf/manifest.xml

+ <hal format="hidl">
+ <name>android.hardware.sensors</name>
+ <transport>hwbinder</transport>
+ <version>1.0</version>
+ <interface>
+ <name>ISensors</name>
+ <instance>default</instance>
+ </interface>
+ </hal>

After adding that, the HAL layer properly communicates the sensors to Android and the light sensor is now available:

7,757 次查看
Pritamsrisahoo_ss
Contributor I

Can you please help me to integrate the lsm6dsm sensor on Android source code and get the values of the sensor in a application.

Steps that i have followed:

1.Driver was loaded and I can get the values in my pc terminal by:cat sys/class/i2c-dev/i2c-2/device/2-006b/iio\:device1/in_accel_x_raw

Then what i need to modify so that to achive the sensor values in any application??

Thankyou in advance..

0 项奖励
回复
12,398 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following community thread where a sensor implementation to the HAL was made: https://community.nxp.com/thread/525702 

Hope it helps.

BR,

Ivan.

0 项奖励
回复