Adding GPIO in device tree error for imx8m mini evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding GPIO in device tree error for imx8m mini evk board

3,693件の閲覧回数
Ruban1
Contributor II

Adding GPIO in device tree error for imx8m mini evk board.

i added 

&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog_1>;

imx8mm-evk {
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO08_GPIO1_IO8 0x19
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41

>;
};

pinctrl_csi_pwn: csi_pwn_grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO07_GPIO1_IO7 0x19
>;
};

}

 

in path arch/arm64/boot/dts/freescale//imx8mm-evk.dts

Error created while building is attached below

The screenshot of added and  screenshot where  the error is showing

Thanks in advance

Regards

Ruban

 

ラベル(1)
0 件の賞賛
返信
1 返信

3,675件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please try to remove "imx8mm-evk {" in your dts file.

For your reference:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8dxl-evk....

 

&iomuxc {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_hog>;

		pinctrl_hog: hoggrp {
			fsl,pins = <
				IMX8DXL_COMP_CTL_GPIO_1V8_3V3_GPIORHB_PAD	0x000514a0
				IMX8DXL_COMP_CTL_GPIO_1V8_3V3_GPIORHK_PAD	0x000014a0
				IMX8DXL_SPI3_CS0_ADMA_ACM_MCLK_OUT1		0x0600004c
				IMX8DXL_SNVS_TAMPER_OUT1_LSIO_GPIO2_IO05_IN	0x0600004c
			>;
		};

		pinctrl_usbotg1: otg1 {
			fsl,pins = <
				IMX8DXL_USB_SS3_TC0_CONN_USB_OTG1_PWR		0x00000021
			>;
		};

0 件の賞賛
返信