Add precompiled Module to Yocto Image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Add precompiled Module to Yocto Image

4,424 次查看
patrick_jakob
Contributor III

Hello Everybody,

I am a little confused about the correct way, how to add a precompiled module to my Yocto Image. I thought the easiest way is to create a new recipe.

Recipe:

-----------------------------------------------------------------------------------------

DESCRIPTION = "Install of several kernel modules"
LICENSE = "CLOSED"

kmoddir = "/lib/modules/${KERNEL_VERSION}/wlan"

SRC_URI = "file://modules/compat.ko \
file://modules/sxcfg80211.ko \
file://modules/wlan.ko \
"

FILES_${PN} += "/lib/modules/ ${kmoddir} ${kmoddir}/compat.ko ${kmoddir}/sxcfg80211.ko ${kmoddir}/wlan.ko"

do_install() {
install -d ${D}${kmoddir}
install -m 0755 ${WORKDIR}/modules/compat.ko ${D}${kmoddir}
install -m 0755 ${WORKDIR}/modules/sxcfg80211.ko ${D}${kmoddir}
install -m 0755 ${WORKDIR}/modules/wlan.ko ${D}${kmoddir}
}

-----------------------------------------------------------------------------------------

The recipe built is successfully, the modules are available in the rootfs, but not at the correct location. The modules are located in "/lib/modules/wlan" but the correct path should be "/lib/modules/KERNEL_VERSION/wlan".

So I checked the ${KERNEL_VERSION} variable and it´s empty. How can I access this variable in my recipe? Do I need a special include?

My second idea was to add the module by inherit module to my recipe. There is also an example located in poky/meta-skeleton/recipes-kernel/hello-mod. My main problem is that the module recipes tries always to compile my own recipe. But there is nothing to compile, my kernel images are precompiled.

So that´s why I am confused and not sure which is the correct approach?

Thanks for any help,

标签 (3)
0 项奖励
回复
1 回复

3,294 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Patrick,

I guess KERNEL_VERSION should be declare or is not part of yocto, you have to use the whole kernel version you are using.

0 项奖励
回复