Add/Edit source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add/Edit source code

1,444 Views
imx7newbie
Contributor II

Hi,

I am using IMX.7 in combination with Yocto Project.

I follow steps mentioned in 

Yocto Project Mega-Manual 

it took 6 hours on ubuntu to compile bsp and built sd card image.

but didn't understand where to add/edit source code lets say for UART/PCIE etc.

Labels (1)
0 Kudos
Reply
1 Reply

1,328 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to "i.MX_BSP_Porting_Guide.pdf".

In particular -  use Chapter 2 (Porting Kernel) and Chapter 3 (Porting U-Boot).

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply