Add CAN Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add CAN Support

Jump to solution
3,746 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on IMX8QM with Android 9. Currently, I am using imx-p9.0.0_2.1.1-auto-ga source. I needs to add CONFIG_CAN_FLEXCAN. But, I am unable to enable.

by using make menuconfig,

 

I got depends on  (ARM || ARM64 || PPC) - I don't how to add this dependency,

   Depends on: NET [=y] && CAN [=y] && CAN_DEV [=y] && (ARM || ARM64 || PPC) 

If I check ARM64,

   CONFIG_ARCH_MXC_ARM64 - CLKSRC_MMIO -etc,

 

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
3,543 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

As my understanding, you do not need to enable any module. Just is saying that the module could work for architectures ARM, ARM64, and Power PC. This is similar when you are initializing the toolchain, you write the macro ARCH=arm, or ARCH=arm64. 

 Best regards,

Diego.

View solution in original post

0 Kudos
Reply
5 Replies
3,543 Views
vinothkumars
Senior Contributor IV

Will you please, provide the sample dotconfig files (included flex can dependency).

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
3,543 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

The (ARM || ARM64 || PPC) is saying that it is supported by the architecture ARM, ARM64 or Power PC. In this case, it is the Architecture ARM64.

Best regards,

Diego.

0 Kudos
Reply
3,543 Views
vinothkumars
Senior Contributor IV

Thank you Diego,

If it possible, Will you please guide me, how to enable ARM64 in Kernel config.

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
3,544 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

As my understanding, you do not need to enable any module. Just is saying that the module could work for architectures ARM, ARM64, and Power PC. This is similar when you are initializing the toolchain, you write the macro ARCH=arm, or ARCH=arm64. 

 Best regards,

Diego.

0 Kudos
Reply
3,543 Views
vinothkumars
Senior Contributor IV

Thank you Diego for your reply.

Thanks @ Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply