Activating of cortex m4 in android 9 based imx8mm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activating of cortex m4 in android 9 based imx8mm

1,340件の閲覧回数
hashir
Contributor I

Hi,

First of all I am new to IMX processors and also Android source.

I am trying to implement cortex m4 for remote control interfacing.

Evk kit provided by MYIR.

Android version - 9

kernel version - 4.14

trying to activate rpmsg in the using "modprobe imx_rpmsg_tty" command but it shows error as below

evk_8mm:/data/local/tmp # modprobe imx_rpmsg_tty
modprobe: /etc/modprobe.conf: No such file or directory
modprobe: /etc/modprobe.d: No such file or directory
modprobe: chdir '/lib/modules/4.14.98'

Kindly support urgently.

thanks in advance.

0 件の賞賛
返信
3 返答(返信)

1,301件の閲覧回数
hashir
Contributor I

Okay thanks for support again,

I was able to write the code for gpio interrupt.

but the interrupt occurs if i run the m4 at uboot before starting the kernel, and does not work when the the kernel is loaded.

is there any way that i can dissable the interrupt clearing on kernel side?

0 件の賞賛
返信

1,318件の閲覧回数
hashir
Contributor I

Thanks , but i got it worked on Android 9 and kernel 4.14.

Can you give me example for GPIO interrupt.

It will be very helpful.

0 件の賞賛
返信

1,326件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You need to upgrade your android to android 10 or android 12 since rpmsg doesn't work on Android 9 and kernel 4.14.

Regardd

0 件の賞賛
返信