Accessing RPMB key in Android 9 and Android 12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing RPMB key in Android 9 and Android 12

2,459件の閲覧回数
herman_lin
Contributor II

Hi NXP,

Based on the information I have, Widevine DRM is based on different TEEs depending on the Android version in NXP i.MX8MQ solution: Android 9 uses OPTEE, while Android 12 uses Trusty.

In our tests, we found that an RPMB key written under the "Android 9 + OPTEE" architecture fails verification when used under the "Android 12 + Trusty" architecture. After tracing the relevant code, it appears that OPTEE and Trusty use different algorithms to generate the RPMB key.

We would like to know whether Widevine DRM feature can work well while upgrading from "Android 9 + OPTEE" to "Android 12 + Trusty"?
If the differences between OPTEE and Trusty are causing Widevine DRM to malfunction after the upgrade to Android 12, is there a patch from NXP that supports Android 12 with OPTEE?

Thanks!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,410件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to change all "setUserAuthenticationRequired(true)" by "setUserAuthenticationRequired(false)" 

 

Regards

0 件の賞賛
返信

2,378件の閲覧回数
herman_lin
Contributor II

Hi BIO,

Let's first clarify one thing: Is it possible to use Widevine DRM with an Android 12 + Trusty environment, even if the RPMB key was originally written in an Android 9 + OP-TEE environment?

Thanks!

0 件の賞賛
返信