About using public and private keys with HAB IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About using public and private keys with HAB IMX6

1,824 Views
PramodKumar
Contributor IV

Hi Yuri ,

Can you please guide me regarding public key and private key , that how to generate these keys and how to use it . Means where we have to put the keys in root file system and how we can do the certification .

Regards ,

Pramod

0 Kudos
Reply
1 Reply

1,591 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following general information about the keys.

Chapter 1. Introduction to Public-Key Cryptography Red Hat Certificate System 9 | Red Hat Customer P... 

  As for signing, applied in the HAB, the following general information may be useful.

https://medium.com/coinmonks/public-key-cryptography-and-digital-signatures-6d81a06c15c4

 There are the following NXP app notes regarding HAB specifics.

https://www.nxp.com/docs/en/application-note/AN4581.pdf

https://www.nxp.com/docs/en/application-note/AN12056.pdf

  Note, the generation of the key pairs  are implemented on a host computer with CST help.

The keys are generated  and located on the host,  and it is customer's responsibility

how to store it in a secure way.   Customers can use the (HSM) approach, described in

CST documentation (cst-3.1.0.tar\release\code\back_end-hsm\doc\)

   Further - public keys are located in target boot signed image and can be checked,

using hashes of the SRK, burned in target fuses (for the SRK) and signatures of CSF and 

image keys (signed by the SRK).  


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------