About uboot2014 support Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About uboot2014 support Android

1,297 Views
jiongzhongliu
Contributor III


I want to use uboot2014 to support android(4.2.2) from SD card.The CPU is IMX6Q

First I change the UBOOT_DIR_TOP/borads.cfg file:

  Active  arm         armv7          mx6         freescale       mx6sabresd          mx6qsabresd                                mx6sabresd:IMX_CONFIG=board/freescale/imx/ddr/mx6q_4x_mt41j128.cfg,MX6Q,DEFAULT_FDT_FILE="imx6q-sabresd_nt.dtb",DDR_MB=1024,SYS_USE_SPINOR,ANDROID_SUPPORT

And I reference "Android_User's_Guide",use android source's script "fsl-sdcard-partition.sh" to make my SD card.

After booting, the uboot log is:

Hit any key to stop autoboot:0

mmc1 is current device

** Unrecognized filesystem type **

** Unrecognized filesystem type **

Booting from net ...

*** ERROR:'ethaddr',not set***

*** ERROR:'ethaddr',not set***

Bad Linux ARM zImage magic!

Is anything else I shall change if the uboot2014 can support IMX6Q android

Labels (3)
0 Kudos
Reply
1 Reply

1,187 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

suggest first to try boot linux L3.0.35_4.0.0 (used with android(4.2.2))

with uboot 2014. Also one can post this to uboot mail list

U-Boot Info Page

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply