About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

1,221 Views
yuuki
Senior Contributor II

Dear all,

We use i.MX6Quad.
We want to use eMMC(JEDEC4.51)device.
And we use eMMC Boot.

However, this eMMC does not support SPI mode.
Can we use this eMMC device?

For the method that eMMC(JEDEC4.51) is used in as 4.x,
I referred to the following URL.

https://community.freescale.com/message/435796#435796

However, We do not know whether we can use eMMC which does not support SPI mode.

If we can use this, can MFG tool write a program in this eMMC?

May I have advice?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Reply

987 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Basically the SPI mode is not needed for eMMC operation with i.MX6.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply