About the performance of secure communication (Open SSL) for i.MX6 Dual Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the performance of secure communication (Open SSL) for i.MX6 Dual Lite

Jump to solution
1,392 Views
yuuki
Senior Contributor II

Dear All,

We would like to support OpenSSL(or OpenVPM) on the system of i.MX6Dual Lite.
We would like to know the CPU load factor and bus load factor about supporting OpenSSL.

Would you provide, if there is any information?

Best Regards,
Yuuki

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,228 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,229 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,229 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

for obtaining first link data below please apply to local FAE since these are

internal closed data.

Re: i.MX 6 CAAM performance

CAAM test application for iMX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply