About the performance of secure communication (Open SSL) for i.MX6 Dual Lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the performance of secure communication (Open SSL) for i.MX6 Dual Lite

跳至解决方案
1,389 次查看
yuuki
Senior Contributor II

Dear All,

We would like to support OpenSSL(or OpenVPM) on the system of i.MX6Dual Lite.
We would like to know the CPU load factor and bus load factor about supporting OpenSSL.

Would you provide, if there is any information?

Best Regards,
Yuuki

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,225 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,226 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,226 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

for obtaining first link data below please apply to local FAE since these are

internal closed data.

Re: i.MX 6 CAAM performance

CAAM test application for iMX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复