About the current consumption under RTC operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the current consumption under RTC operation

ソリューションへジャンプ
2,425件の閲覧回数
george
Senior Contributor II

Dear All,

We want to calculate the life of a Back-up battery when using i.MX6 with RTC 32k X'tal.

The datasheet has two descriptions about it.

=> http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC

Though described as 41uA in IMX6SDLCEC Page 30, Is it this?

Or should it calculate from the description in Page38? (4uA + 20uA + 1.5uA)

Best Regards,

George

ラベル(1)
0 件の賞賛
返信
1 解決策
2,220件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

correct reading as described : 41uA in IMX6SDLCEC Page 30.

Page38 gives description just separate OSC32K block.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,221件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

correct reading as described : 41uA in IMX6SDLCEC Page 30.

Page38 gives description just separate OSC32K block.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,220件の閲覧回数
george
Senior Contributor II

Dear Igor,

Thanks.

I understood.

BR,

George

0 件の賞賛
返信