About the ability to run custom applications without using an external ROM on i. MX6 Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the ability to run custom applications without using an external ROM on i. MX6 Solo

ソリューションへジャンプ
1,996件の閲覧回数
azausatu
Contributor I

Hello!

I use a processor i.MX 6 Solo. I want to run my applications without using external RAM and ROM memory, without operating systems, bare metal.

Questions:
1) does the processor have internal ROM memory for storing user applications?
2) If the application can be loaded into internal permanent memory, please give information on how to do this. Use mfgtool? How do I configure booting from internal memory?
3) i.MX 6 Solo can only be used with external permanent memory?


Thank you very much!
I apologize for the stupid questions.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
1,877件の閲覧回数
kunalkotecha1
Senior Contributor II

Hi Azamat G.,

I believe internal ROM is the Read-Only Memory and won't be able to use the same for flashing an application. Below is the screenshot of available boot devices. Please refer to section 8.5 of the attached Reference Manual for further details.

pastedImage_1.png

Let us know if you have any further queries on the same.

Regards,

Kunal

元の投稿で解決策を見る

1 返信
1,878件の閲覧回数
kunalkotecha1
Senior Contributor II

Hi Azamat G.,

I believe internal ROM is the Read-Only Memory and won't be able to use the same for flashing an application. Below is the screenshot of available boot devices. Please refer to section 8.5 of the attached Reference Manual for further details.

pastedImage_1.png

Let us know if you have any further queries on the same.

Regards,

Kunal